Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
System is a Win7 64bits, fully up to date. CCS 6.2 runs perfectly on it.
Tried to install both the online and the offline packages, but they come to the same error: 'can't read "update": no such variable'.
The logs don't seem to say much, but I can add here if useful. The files get copied, but I don't see a ccstudio.exe inside the /eclipse folder.
One more point: the zipped file says Win32, there seems to be no other option on the download links - should there be a Win64?
Image of the error follows: