Hi there,
I am running win xp sp3, with CCS Core 4.1.2.00027.
I am using the F283x CPU Cycle Accurate Simulator.
When running the program, I cannot make the profile clock indicator update - it is always stuck at 0.
The program is stepping through the code and updating variables, just not the clock cycles.
I've noticed in my clock setup that there is no Instruction Cycle Time or Pipeline Adjustments field like in spru328b.pdf page 150 (see below for pic).
Is the profile clock unsupported? I am using a standard 2833x example code and configuration.