This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP430I2041: Can't debug the MSP430I2041 with ez Fet Lite

Part Number: MSP430I2041
Other Parts Discussed in Thread: MSP430F5529, , MSP430G2553

Tool/software: Code Composer Studio

Hi,

I'm trying to use the ez Fet Lite debugger from the MSP430F5529 Launchpad to program the MSP430I2041. I'm using CCS v7.0.0.00033

When I start the debugger I get the following error:

MSP430: File Loader: Verification failed: Values at address 0x8000 do not match Please verify target memory and memory map.

I also tried the same ez Fet Lite with an MSP430G2553. It works without any problem.

The code in both cases the supplied Blinky example.

Anybody has any idea on it?

Thanks,

Zoltan