This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: how to use example file on TI website? *(audio example)

Tool/software: Code Composer Studio

I already installed BIOSPSP_01_30_01_Setup uploaded on TI site

i wanna compile the project in 

C:\Program Files\Texas Instruments\pspdrivers_01_30_01\packages\ti\pspiom\examples\evm6747\audio\build\cc3\audioSample.pjt

but when i compile the pjt file, mcasp error is ocurred. so i downloaded the EDMA3.LLD.setupwin32_01_11_03_11.

then, another error is occured. it is "SWI_new" overflowed;

how can i fix it? 

  • Hello,

    Because you mention *.pjt file, I assume you are using CCSv3.3. Note that this version of CCS, and also the version of BIOSPSP you are using, is very old and no longer supported. You can try the TI-RTOS forum to see if the experts there can provide some suggestions.

    Is there any reason why you are using such old version?

    Thanks

    ki

  • Thanks your reply.

    You are right, i am using CCSv3.3. There is no important reason why i am using old version.
    I just use CCS and BIOSPSP version installed in my laptop.

    So, do i have to change my programs to new version for compile audiosample.pjt?
    Then, how can i get new version programs on TI website?

    SH
  • i found that C6747 needs to use only CCS v4.0.2. So i installed it.
    Then i imported audiosample.pjt which is set up from BIOSPSP_01_30_01_Setup file.

    Is this BIOSPSP_01_30_01_Setup file is new one? is it okay? Beacuse of this pjt, error is occured contineously.
  • Hello,
    I would suggest posting in the C674x forum for suggestions on how to proceed. The experts there can best recommend what versions of the tools and what software packages are best to use. The versions you are mentioning now are quite old and I want to make sure you use the most relevant versions for your device.

    e2e.ti.com/.../42

    Thanks
    ki