Other Parts Discussed in Thread: MSP430F5359, MSP430WARE
Tool/software: Code Composer Studio
Hello,
I have an issue compiling an empty project with CCS5 and MSP430Ware driver lib version 2.80.00.01 with an MSP430F5359 selected.
The empty project is created via CCS -> View -> Ti resource explorer -> MSP430Ware -> Libraries -> Driver Library -> MSP430F5xx_6xx -> empty project. click on: Step 1: Import the example project into CCS.
When I compile this newly created project, no errors are reported, however when I change the msp part to via the projecty properties to an MSP430F5359, and I complile the project, 2 errors are reported:
Description Resource Path Location Type
#20 identifier "LDOOEN_H" is undefined ldopwr.c /emptyProject/driverlib/MSP430F5xx_6xx line 152 C/C++ Problem
#20 identifier "LDOOEN_H" is undefined ldopwr.c /emptyProject/driverlib/MSP430F5xx_6xx line 157 C/C++ Problem
A lillte help would be welcome
| Step 1: |