This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2650: Can't Connect to CC2650

Part Number: CC2650

Tool/software: Code Composer Studio

Hi all.

I have build my own cc2650 hardware, it's basically the same scheme of the cc2650 launcphad.

I am facing a weird problem:

I download the app server example app to flash then the spp server stack but I can't see my device within Bluetooth network.

Just for information: When I download the app the current supply is 2 mA and when I download the stack is about 4 mA. In both cases looks like the radio isn't working.

My example works fine with the lauchpad.

Another information is that I can't put a breakpoint on the server task, the program don't execute the code relative to the server.

Is there a way to download both app and stack in a row using ccs? It's looking like only the app or the stack is running, not both.

Thanks