This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/PGA970EVM: Code Composer Studio does not have ti-cgt-arm_5.2.6 folder

Part Number: PGA970EVM

Tool/software: TI C/C++ Compiler

I have PGA970EVM which is based on M0 core. I downloaded the code from TI website and when trying to compile it, I realised that the CCS install directory structure does not have the folder i-cgt-arm_5.2.6 which is supposed to contain the rtsv6M0_T_le_eabi.lib file. I have CCS versions 6.1 and 7.0 and neither of these installations have it.

  • You can use the CCS update feature to obtain older versions of the ARM compiler.  Please see this wiki article about changing compiler versions.  

    Instead of using version 5.2.6, consider using the latest 5.2.x version (presently 5.2.8).  It is exactly the same as 5.2.6, but with more bug fixes.

    Thanks and regards,

    -George