Other Parts Discussed in Thread: EK-TM4C123GXL
Tool/software: Linux
Hi all,
In the last days I'm facing with a boring situation on my CCSv6.2.0.00050 installed on an Ubuntu 15.10 laptop.
I'm using the TivaC launchpad and, while in the last week i could use my ccs with no problem, now I have an unusual problem with the debugger, because I can't launch anymore debugger session.
I program using assembly only language: TI v15.12.3.LTS but, while the compiler goes without any problem, the debugger doesn't.
I tried almost anything, switched to CCSv7, bought another launchpad, used another USB cable, reinstalled all the Operating system, but whenever I go and whatever I do, the result is ever the same:
"Error connecting to the target" prompt as soon as I launch the debugger.
Searching on internet and on my system, I found an applet inside my installation directory, under: <install dir>/ccsv6/ccs_base/common/uscif/xds100serial, which says to me: "No XDS100 emulators were found on the system" but I don't understood: if I'm using the launchpad, my emulators shouldn't be the "Stellaris In circuit Debugger"? Is normal in my case that this application don't found the xds100 emulators?
Following this forum thread:

seems, that "Steven Hansen" got a very similar problem to mine, but finally he get back to a Windows system, but I can't, so I havo absolutely to fix the problem.
I also found some strange issues on my USB ports, and attached to this message a full report of my usb ports, and seems that the Stellaris emulator, trigger a serial link that is called, in my system: "ttyACM0", is this correct? Because in the forum post that I linked just before, seems that It has to be a "ttyUSB0" instead, so which must be the correct setup of CCS under linux to get a debugger up and running?
I also tried to manually unbind the launchpad from the "cdc_acm" usb driver, to manually bind it in "ftdi_sio" driver, or "usbserial" one, but it failed, because the binding to the new driver fails.
Please help me!
Please point me towards some new check to perform, or some other way, beacause now I don'tknow how could I do, to fix my debugger.
Thanks
monitor will print the received events for: UDEV - the event which udev sends out after rule processing KERNEL - the kernel uevent KERNEL[176.022315] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2 (usb) ACTION=add BUSNUM=004 DEVNAME=/dev/bus/usb/004/003 DEVNUM=003 DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2 DEVTYPE=usb_device MAJOR=189 MINOR=386 PRODUCT=1cbe/fd/100 SEQNUM=2456 SUBSYSTEM=usb TYPE=239/2/1 KERNEL[176.023510] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.0 (usb) ACTION=add DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.0 DEVTYPE=usb_interface INTERFACE=2/2/1 MODALIAS=usb:v1CBEp00FDd0100dcEFdsc02dp01ic02isc02ip01in00 PRODUCT=1cbe/fd/100 SEQNUM=2457 SUBSYSTEM=usb TYPE=239/2/1 KERNEL[176.026303] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.0/tty/ttyACM0 (tty) ACTION=add DEVNAME=/dev/ttyACM0 DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.0/tty/ttyACM0 MAJOR=166 MINOR=0 SEQNUM=2458 SUBSYSTEM=tty KERNEL[176.026644] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.1 (usb) ACTION=add DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.1 DEVTYPE=usb_interface DRIVER=cdc_acm INTERFACE=10/0/0 MODALIAS=usb:v1CBEp00FDd0100dcEFdsc02dp01ic0Aisc00ip00in01 PRODUCT=1cbe/fd/100 SEQNUM=2459 SUBSYSTEM=usb TYPE=239/2/1 KERNEL[176.027077] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.2 (usb) ACTION=add DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.2 DEVTYPE=usb_interface INTERFACE=255/0/0 MODALIAS=usb:v1CBEp00FDd0100dcEFdsc02dp01icFFisc00ip00in02 PRODUCT=1cbe/fd/100 SEQNUM=2460 SUBSYSTEM=usb TYPE=239/2/1 KERNEL[176.027444] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.3 (usb) ACTION=add DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.3 DEVTYPE=usb_interface INTERFACE=254/1/1 MODALIAS=usb:v1CBEp00FDd0100dcEFdsc02dp01icFEisc01ip01in03 PRODUCT=1cbe/fd/100 SEQNUM=2461 SUBSYSTEM=usb TYPE=239/2/1 UDEV [176.034435] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2 (usb) ACTION=add BUSNUM=004 DEVNAME=/dev/bus/usb/004/003 DEVNUM=003 DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2 DEVTYPE=usb_device DRIVER=usb ID_BUS=usb ID_MM_DEVICE_IGNORE=1 ID_MODEL=In-Circuit_Debug_Interface ID_MODEL_ENC=In-Circuit\x20Debug\x20Interface ID_MODEL_FROM_DATABASE=In-Circuit Debug Interface ID_MODEL_ID=00fd ID_REVISION=0100 ID_SERIAL=Texas_Instruments_In-Circuit_Debug_Interface_0E208121 ID_SERIAL_SHORT=0E208121 ID_USB_INTERFACES=:020201:0a0000:ff0000:fe0101: ID_VENDOR=Texas_Instruments ID_VENDOR_ENC=Texas\x20Instruments ID_VENDOR_FROM_DATABASE=Luminary Micro Inc. ID_VENDOR_ID=1cbe MAJOR=189 MINOR=386 PRODUCT=1cbe/fd/100 SEQNUM=2456 SUBSYSTEM=usb TYPE=239/2/1 USEC_INITIALIZED=176033739 UDEV [176.051914] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.0 (usb) ACTION=add DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.0 DEVTYPE=usb_interface DRIVER=cdc_acm ID_MODEL_FROM_DATABASE=In-Circuit Debug Interface ID_USB_CLASS_FROM_DATABASE=Miscellaneous Device ID_USB_PROTOCOL_FROM_DATABASE=Interface Association ID_VENDOR_FROM_DATABASE=Luminary Micro Inc. INTERFACE=2/2/1 MODALIAS=usb:v1CBEp00FDd0100dcEFdsc02dp01ic02isc02ip01in00 PRODUCT=1cbe/fd/100 SEQNUM=2457 SUBSYSTEM=usb TYPE=239/2/1 USEC_INITIALIZED=176043482 UDEV [176.053569] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.1 (usb) ACTION=add DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.1 DEVTYPE=usb_interface DRIVER=cdc_acm ID_MODEL_FROM_DATABASE=In-Circuit Debug Interface ID_USB_CLASS_FROM_DATABASE=Miscellaneous Device ID_USB_PROTOCOL_FROM_DATABASE=Interface Association ID_VENDOR_FROM_DATABASE=Luminary Micro Inc. INTERFACE=10/0/0 MODALIAS=usb:v1CBEp00FDd0100dcEFdsc02dp01ic0Aisc00ip00in01 PRODUCT=1cbe/fd/100 SEQNUM=2459 SUBSYSTEM=usb TYPE=239/2/1 USEC_INITIALIZED=176045669 UDEV [176.053745] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.2 (usb) ACTION=add DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.2 DEVTYPE=usb_interface ID_MODEL_FROM_DATABASE=In-Circuit Debug Interface ID_USB_CLASS_FROM_DATABASE=Miscellaneous Device ID_USB_PROTOCOL_FROM_DATABASE=Interface Association ID_VENDOR_FROM_DATABASE=Luminary Micro Inc. INTERFACE=255/0/0 MODALIAS=usb:v1CBEp00FDd0100dcEFdsc02dp01icFFisc00ip00in02 PRODUCT=1cbe/fd/100 SEQNUM=2460 SUBSYSTEM=usb TYPE=239/2/1 USEC_INITIALIZED=176047657 UDEV [176.053906] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.3 (usb) ACTION=add DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.3 DEVTYPE=usb_interface ID_MODEL_FROM_DATABASE=In-Circuit Debug Interface ID_USB_CLASS_FROM_DATABASE=Miscellaneous Device ID_USB_PROTOCOL_FROM_DATABASE=Interface Association ID_VENDOR_FROM_DATABASE=Luminary Micro Inc. INTERFACE=254/1/1 MODALIAS=usb:v1CBEp00FDd0100dcEFdsc02dp01icFEisc01ip01in03 PRODUCT=1cbe/fd/100 SEQNUM=2461 SUBSYSTEM=usb TYPE=239/2/1 USEC_INITIALIZED=176049292 UDEV [176.059616] add /devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.0/tty/ttyACM0 (tty) ACTION=add DEVLINKS=/dev/serial/by-id/pci-Texas_Instruments_In-Circuit_Debug_Interface_0E208121-if00 /dev/serial/by-path/pci-0000:00:1a.1-usb-0:2:1.0 DEVNAME=/dev/ttyACM0 DEVPATH=/devices/pci0000:00/0000:00:1a.1/usb4/4-2/4-2:1.0/tty/ttyACM0 ID_BUS=pci ID_MM_CANDIDATE=1 ID_MODEL=In-Circuit_Debug_Interface ID_MODEL_ENC=In-Circuit\x20Debug\x20Interface ID_MODEL_FROM_DATABASE=In-Circuit Debug Interface ID_MODEL_ID=0x2938 ID_PATH=pci-0000:00:1a.1-usb-0:2:1.0 ID_PATH_TAG=pci-0000_00_1a_1-usb-0_2_1_0 ID_PCI_CLASS_FROM_DATABASE=Serial bus controller ID_PCI_INTERFACE_FROM_DATABASE=UHCI ID_PCI_SUBCLASS_FROM_DATABASE=USB controller ID_REVISION=0100 ID_SERIAL=Texas_Instruments_In-Circuit_Debug_Interface_0E208121 ID_SERIAL_SHORT=0E208121 ID_TYPE=generic ID_USB_CLASS_FROM_DATABASE=Miscellaneous Device ID_USB_DRIVER=cdc_acm ID_USB_INTERFACES=:020201:0a0000:ff0000:fe0101: ID_USB_INTERFACE_NUM=00 ID_USB_PROTOCOL_FROM_DATABASE=Interface Association ID_VENDOR=Texas_Instruments ID_VENDOR_ENC=Texas\x20Instruments ID_VENDOR_FROM_DATABASE=Luminary Micro Inc. ID_VENDOR_ID=0x8086 MAJOR=166 MINOR=0 SEQNUM=2458 SUBSYSTEM=tty TAGS=:systemd: USEC_INITIALIZED=176055574