Part Number: TMS320F28335
Other Parts Discussed in Thread: CONTROLSUITE, ADS8329
Tool/software: Code Composer Studio
Hello,
I have still issue with C28xxx FastRTS-Library.
I've copied the source files like sin_f32.asm cos_f32.asm sqrt_f32.asm direct to my project src directory.
I do this to be able to copy the functions into the RAM after program start.
All these asemmbler files are translatet to object-files, but there is a remaining conflict with sin and cos functions.
With CCS6 compiling I've got the error messages like:
#10056 symbol "_cos" redefined: first defined in "<whole-program>"; redefined in "./src/cos_f32.obj"
#10056 symbol "_sin" redefined: first defined in "<whole-program>"; redefined in "./src/sin_f32.obj"
But all other files/funcition work so far (e.G. sqrt_f32.asm)
What could cause this? I tried several compiler switches, no success.
Or how can I replace the library functions with the fast replacements from sin_f32.asm and cos_f32.asm?
br Ralf