Tool/software: TI C/C++ Compiler
INTERNAL ERROR: C:\ti\ccsv6\tools\compiler\ti-cgt-arm_15.12.1.LTS\bin\armlnk.exe experienced an unhandled exception
This is caused by a defect in the compiler itself. TI Customer
Support may be able to suggest a workaround to avoid this.
Upgrading to the newest version of the compiler may fix this problem.
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue". Include this ENTIRE error message and a
copy of the .pp file created when option --preproc_with_comment
(-ppc) is used.
>> Compilation failure
gmake: *** [RoyaleIII_boot.out] Error 1
gmake: Target `all' not remade because of errors.
FULL BUILD LISTING FOLLOWS:
**** Build of configuration Debug for project boot_uart **** "C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all 'Building file: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_check.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="bl_check.pp" "C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_check.c" 'Finished building: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_check.c' ' ' 'Building file: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_flash.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="bl_flash.pp" "C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_flash.c" 'Finished building: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_flash.c' ' ' 'Building file: ../bl_main_tiva.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="bl_main_tiva.pp" "../bl_main_tiva.c" 'Finished building: ../bl_main_tiva.c' ' ' 'Building file: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_packet.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="bl_packet.pp" "C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_packet.c" 'Finished building: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_packet.c' ' ' 'Building file: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_startup_ccs.s' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="bl_startup_ccs.pp" "C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_startup_ccs.s" "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 190 (col. 14): warning: function-like macro 'INT8_C(value)' ignored during assembly header translation "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 191 (col. 13): warning: function-like macro 'UINT8_C(value)' ignored during assembly header translation "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 192 (col. 14): warning: function-like macro 'INT16_C(value)' ignored during assembly header translation "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 193 (col. 13): warning: function-like macro 'UINT16_C(value)' ignored during assembly header translation "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 194 (col. 14): warning: function-like macro 'INT32_C(value)' ignored during assembly header translation "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 195 (col. 13): warning: function-like macro 'UINT32_C(value)' ignored during assembly header translation "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 198 (col. 14): warning: function-like macro 'INT64_C(value)' ignored during assembly header translation "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 199 (col. 13): warning: function-like macro 'UINT64_C(value)' ignored during assembly header translation "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 203 (col. 14): warning: function-like macro 'INTMAX_C(value)' ignored during assembly header translation "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include/stdint.h", line 204 (col. 13): warning: function-like macro 'UINTMAX_C(value)' ignored during assembly header translation 'Finished building: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_startup_ccs.s' ' ' 'Building file: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_uart.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="bl_uart.pp" "C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_uart.c" 'Finished building: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/boot_loader/bl_uart.c' ' ' 'Building file: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/gpio.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="gpio.pp" "C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/gpio.c" 'Finished building: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/gpio.c' ' ' 'Building file: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/sw_crc.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="sw_crc.pp" "C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/sw_crc.c" 'Finished building: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/sw_crc.c' ' ' 'Building file: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/sysctl.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="sysctl.pp" "C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/sysctl.c" 'Finished building: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/sysctl.c' ' ' 'Building file: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/uart.c' 'Invoking: ARM Compiler' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --include_path="C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/bootloaders/boot_FCC/ccs" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare" --include_path="C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib" -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual --preproc_with_compile --preproc_dependency="uart.pp" "C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/uart.c" 'Finished building: C:/Projects/AMI_Fuel_Cel/Royalle_III_code/trunk/depend/tivaWare/driverlib/uart.c' ' ' 'Building target: RoyaleIII_boot.out' 'Invoking: ARM Linker' "C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 -g --gcc --define=ccs --define=ccs="ccs" --define=PART_TM4C1294NCPDT --diag_warning=225 --gen_func_subsections=on --abi=eabi --ual -z -m"RoyaleIII_boot.map" --stack_size=512 --heap_size=0 -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/lib" -i"C:/ti/ccsv6/tools/compiler/ti-cgt-arm_15.12.1.LTS/include" --reread_libs --warn_sections --xml_link_info="boot_uart_linkInfo.xml" -o "RoyaleIII_boot.out" "./bl_check.obj" "./bl_flash.obj" "./bl_main_tiva.obj" "./bl_packet.obj" "./bl_startup_ccs.obj" "./bl_uart.obj" "./gpio.obj" "./sw_crc.obj" "./sysctl.obj" "./uart.obj" "../tm4c1294ncpdt.cmd" -l"libc.a" <Linking> INTERNAL ERROR: C:\ti\ccsv6\tools\compiler\ti-cgt-arm_15.12.1.LTS\bin\armlnk.exe experienced an unhandled exception This is caused by a defect in the compiler itself. TI Customer Support may be able to suggest a workaround to avoid this. Upgrading to the newest version of the compiler may fix this problem. Contact TI in the E2E support forums at http://e2e.ti.com under "Development Tools", "TI C/C++ Compiler". See the link titled "Submitting an issue". Include this ENTIRE error message and a copy of the .pp file created when option --preproc_with_comment (-ppc) is used. >> Compilation failure gmake: *** [RoyaleIII_boot.out] Error 1 gmake: Target `all' not remade because of errors. **** Build Finished ****