This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377S: CCS/CCSTUDIO: CLA / CCS V.6/LAUNCHXL-F28377S => Mistake in Program Loading

Part Number: TMS320F28377S

Tool/software: Code Composer Studio

Hello Folks,

i´m triying to get the CLA running on a LAUNCHXL-FS28377S - i tried really hard and read a lot, but i can´t make it run.
Is there a way to find out where the problem begins?

For example, how do i know, the CLA compiler actually takes the defined .cla file. I think in the object file schould be some kind of content. Can i distinguish if it worked, or just zeroed (for example)Or perhaps it starts at a different stage at the Linker command file.
Or may be it´s an issue with program RAM assigment to the CLA?

There is a related thread of mine (which is more about getting a specific solution). This one is more about to find the root of the evil ;>
e2e.ti.com/.../563082

Best regards,

Jasson