Part Number: MSP430G2553
Tool/software: Code Composer Studio
Hi,
I would like to generate a matrix of binary random numbers and then display the matrix on the debug console. Here is the my code:
//RNG
#include "msp430G2553.h"
#include <stdint.h>
#include <stdlib.h>
#include <stdio.h>
void main( void )
{
WDTCTL = (WDTPW | WDTHOLD); // Stop watchdog timer
BCSCTL1 = CALBC1_16MHZ; // Set range to 16MHz
DCOCTL = CALDCO_16MHZ; // Set DCO step and modulation to 16MHz
TA0CCR0 = 400; // Frequency 40kHz, 25us
TA0CCTL1 = OUTMOD_7; // Reset / set
TA0CTL = (TASSEL_2 | ID_0 | MC_1 | TACLR | TAIE); // SMCLK, divider 1, up-mode, clear, interrupt enabled
_BIS_SR(GIE); // Enable global interrupts
while( 1 ); // Endless loop
}
// Timer0 A1 interrupt service routine
#pragma vector = TIMER0_A1_VECTOR
__interrupt void Timer0_A1_ISR( void )
{
static uint8_t x = 4;
static uint8_t y = 8;
static uint8_t i = 0;
static uint8_t p = 0;
static uint8_t random = 0;
static uint8_t randomNums [4][8] = {{0}};
for ( i = 0; i < x; i++)
{
// This loop is for the row
for ( p = 0; p < y; p++)
{
//randomize each element for the array.
random = rand() % 1;
randomNums[i][p] = random;
printf ("binary: %s\n",randomNums[i][p]);
}
}
}
Using the above code, I get this error: "program will not fit into available memory". I have read the following guide describing how to use printf in CCSV 4 and 5:
http://processors.wiki.ti.com/index.php/Printf_support_for_MSP430_CCSTUDIO_compiler
However, I am using CCSV6.2 and the settings in properties are different than what is shown in the above link and I can not find a way to increase the heap memory size (I think that might be why I am getting the error).
Can you please help me resolve this issue.
Thank you very much!