This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3100BOOST: Getting Started with P2P - "Missing separator" error running CCS debug session (Windows 10)

Part Number: CC3100BOOST
Other Parts Discussed in Thread: CC3100

Tool/software: Code Composer Studio

Hi all,

I have the P2P example nearly working with my CC3100's and MSP40FR5969's.

Every time I compile the program it gives a "missing separator"  error in the spi.d file in the Debug folder. I have found a fix for this, here:

Is there a way to fix this without having to remove the spaces from the file after every compilation?

Thanks in advance,

Ciaran

  • Hi Ciaran,

    What version of CCS, MSP430 compiler, and CC3100 SDK version are you using?

    I was able to compile the p2p example from the CC3100 SDK v1.2 on CCS v6.2 with the most recent MSP430 compiler v16.12.0.STS without any issues or changes.

    Best regards,
    Sarah
  • Hi Sarah,

    I'm using CCS version 6.1.3, CC3100 SKD version 1.2 and a stupidly out of date MSP430 compiler version 4.3.1.
    Currently updating to the compiler v16.12.

    Thanks for the help :)
    Ciaran
  • Hi Sarah,

    I can now compile the example but the error seems to happen when I start to debug the design. I'll then get the missing separator error, if I change the spi.d file then I can download it to the board. But I have to alter this file after every compile and before every debug session.

    Thanks again,
    Ciaran
  • Hi Ciaran,

    Unfortunately, I'm not seeing the same issue on my setup. I would suggest upgrading to the most recent CCS version, as it may be a debugger error. You should also be sure that the most recent service pack is on the CC3100. You can also download a clean version of the SDK in case your version has been corrupted somehow.

    Best regards,
    Sarah
  • Hi Sarah,

    I have downloaded the latest CCS v7.0 and the sdk for the CC3100. I am still getting the same behavior. Would you be able to send me your exact set up just encase I messing something up. Out of interest could this be a windows 10 issue?

    I'm lost for ideas on this one!

    Thanks,
    Ciaran
  • Hi Ciaran,

    I've run this on both CCS v6.2 and v7.0, with CC3100 SDK v1.2 and the most recent service pack, and TI v16.9.0.LTS compiler. I am on a Windows 7 machine.

    This does sound like a continuing compiler/CCS debugger issue, so I'm going to move this post over to their forum so you get a faster answer.

    Best regards,
    Sarah

  • Hi Sarah,

    That would be great, thanks a million for you help :)

    Ciaran