This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCS 5.5.0 -> Error: Program "make" is not found in PATH

Genius 4170 points

Tool/software: Code Composer Studio

Hello,

just wondering i got this issue out of the blue, worked properly half year ago, now i am normally working in CCS 6.x now but some of our older products still need CCS5.5 since the code is from there.

Now I cannot see my workspaces anymore, and i cannot built the files. a collegue of mine had this problemwith version 6 also a month ago, what could be the issue for that???

I like software that just changes over time due to windows updates or some other voodoo stuff..

cheers

  • Hello,
    Please see the below url for some suggestions:
    processors.wiki.ti.com/.../Build_Errors_in_CCS

    Also make sure your workspace path does not have any non-alphanumeric characters:
    processors.wiki.ti.com/.../Build_Errors_in_CCS

    Hope this helps
    ki
  • I kind of read that, and did already build another workspace and imported my old file into that, same error.

    Waht is really confusing and haunts me the last couple of years, which is why i suspect all software development from your side as well as windows is the following:

    I use a working CCS workspace with a working program code, and after 6 month i try to use the exact thing again and it simply does not work anymore, i am highly suspicious of windows updates int he meantime and maybe some CCS updates too. And I assume I am not the only one with this opinion.

    Anyway I got my workarounds with flashing the out file directly without debug possibilities into the MSP, but of course that is really just a workaround.