This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO-C2000: Problem to connect CCS v7 via SD XDS560 to 28075 control card

Part Number: CCSTUDIO-C2000

Tool/software: Code Composer Studio

Hi,

I have problems to connect CCS v 7.0.0.00042 to my 28075 control card via a Spectrum Digital XDS 560 v2 LC Traveller. I have no problems with my old CCS v 6.1.1.00022 (and the same HW). Below are the reports of the 'Test Connection' and the ccxml file.


Trying to connect CCS v7 to the target yields:

Connect to device:

C28xx_CPU1: Error connecting to the target: (Error -1155 @ 0x0) Device may be operating in low-power mode. The debugger has forced the device to wake up. Choose 'OK' to attempt to complete the debug connection. (Emulation package 6.0.504.1)

Any idea what's wrong?


Thanks,

Frank

CCS 7.0.0.00042 report:

[Start: Spectrum Digital XDS560V2 STM TRAVELER Emulator]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\F54A0~1.MOL\AppData\Local\TEXASI~1\
    CCS\ti\3\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
The library build date was 'Dec  9 2016'.
The library build time was '11:46:58'.
The library package version is '6.0.504.1'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '6' (0x00000006).
The controller has an insertion length of '0' (0x00000000).
The cable+pod has a version number of '8' (0x00000008).
The cable+pod has a capability number of '7423' (0x00001cff).
This utility will attempt to reset the controller.

A error occurred while attempting to reset the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-128' (0xffffff80).
The title is 'SC_ERR_CMD_INVALID_MULT'.

The explanation is:
Unified-SCIF is operating in multiple client mode.
The operation being attempted is invalid in this mode.
It is likely a problem with `SC_CMD' in SMG_call().

[End: Spectrum Digital XDS560V2 STM TRAVELER Emulator]


CCS 6.1.1. report:

[Start: Spectrum Digital XDS560V2 STM TRAVELER Emulator_0]

Execute the command:

%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

C:\Users\F54A0~1.MOL\AppData\Local\TEXASI~1\
    CCS\ti\0\0\BrdDat\testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 560/2xx-class product.
This utility will load the program 'sd560v2u.out'.
Loaded FPGA Image: C:\ti\ccsv6\ccs_base\common\uscif\dtc_topx16.jbc
The library build date was 'Oct  6 2016'.
The library build time was '19:16:59'.
The library package version is '6.0.407.6'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '6' (0x00000006).
The controller has an insertion length of '0' (0x00000000).
The cable+pod has a version number of '8' (0x00000008).
The cable+pod has a capability number of '7423' (0x00001cff).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the Nano-TBC VHDL.
The link is a 560-class second-generation-560 cable.
The software is configured for Nano-TBC VHDL features.
The controller will be software reset via its registers.
The controller has a logic ONE on its EMU[0] input pin.
The controller has a logic ONE on its EMU[1] input pin.
The controller will use falling-edge timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '2' (0x0002).
The utility logic has not previously detected a power-loss.
The utility logic is not currently detecting a power-loss.
Loaded FPGA Image: C:\ti\ccsv6\ccs_base\common\uscif\dtc_topx16.jbc

-----[The log-file for the JTAG TCLK output generated from the PLL]----------

  Test  Size   Coord      MHz    Flag  Result       Description
  ~~~~  ~~~~  ~~~~~~~  ~~~~~~~~  ~~~~  ~~~~~~~~~~~  ~~~~~~~~~~~~~~~~~~~
    1   none  - 01 00  500.0kHz   -    similar      isit internal clock
    2   none  - 01 09  570.3kHz   -    similar      isit internal clock
    3     64  - 01 00  500.0kHz   O    good value   measure path length
    4     16  - 01 00  500.0kHz   O    good value   auto step initial
    5     16  - 01 0D  601.6kHz   O    good value   auto step delta
    6     16  - 01 1C  718.8kHz   O    good value   auto step delta
    7     16  - 01 2E  859.4kHz   O    good value   auto step delta
    8     16  + 00 02  1.031MHz   O    good value   auto step delta
    9     16  + 00 0F  1.234MHz   O    good value   auto step delta
   10     16  + 00 1F  1.484MHz   O    good value   auto step delta
   11     16  + 00 32  1.781MHz   O    good value   auto step delta
   12     16  + 01 04  2.125MHz   O    good value   auto step delta
   13     16  + 01 11  2.531MHz   O    good value   auto step delta
   14     16  + 01 21  3.031MHz   O    good value   auto step delta
   15     16  + 01 34  3.625MHz   O    good value   auto step delta
   16     16  + 02 05  4.313MHz   O    good value   auto step delta
   17     16  + 02 13  5.188MHz   O    good value   auto step delta
   18     16  + 02 23  6.188MHz   O    good value   auto step delta
   19     16  + 02 37  7.438MHz   O    good value   auto step delta
   20     16  + 03 07  8.875MHz   O    good value   auto step delta
   21     16  + 03 15  10.63MHz   O    good value   auto step delta
   22     16  + 03 1E  11.75MHz  {O}   good value   auto step delta
   23     64  + 02 3E  7.875MHz   O    good value   auto power initial
   24     64  + 03 0E  9.750MHz   O    good value   auto power delta
   25     64  + 03 16  10.75MHz   O    good value   auto power delta
   26     64  + 03 1A  11.25MHz   O    good value   auto power delta
   27     64  + 03 1C  11.50MHz   O    good value   auto power delta
   28     64  + 03 1D  11.63MHz   O    good value   auto power delta
   29     64  + 03 1D  11.63MHz   O    good value   auto power delta
   30     64  + 03 13  10.38MHz  {O}   good value   auto margin initial

The first internal/external clock test resuts are:
The expect frequency was 500000Hz.
The actual frequency was 499110Hz.
The delta frequency was 890Hz.

The second internal/external clock test resuts are:
The expect frequency was 570312Hz.
The actual frequency was 569214Hz.
The delta frequency was 1098Hz.

In the scan-path tests:
The test length was 2048 bits.
The JTAG IR length was 6 bits.
The JTAG DR length was 1 bits.

The IR/DR scan-path tests used 30 frequencies.
The IR/DR scan-path tests used 500.0kHz as the initial frequency.
The IR/DR scan-path tests used 11.75MHz as the highest frequency.
The IR/DR scan-path tests used 10.38MHz as the final frequency.

-----[Measure the source and frequency of the final JTAG TCLKR input]--------

The frequency of the JTAG TCLKR input is measured as 10.37MHz.

The frequency of the JTAG TCLKR input and TCLKO output signals are similar.
The target system likely uses the TCLKO output from the emulator PLL.

-----[Perform the standard path-length test on the JTAG IR and DR]-----------

This path-length test uses blocks of 64 32-bit words.

The test for the JTAG IR instruction path-length succeeded.
The JTAG IR instruction path-length is 6 bits.

The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 1 bits.

-----[Perform the Integrity scan-test on the JTAG IR]------------------------

This test will use blocks of 64 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.

The JTAG IR Integrity scan-test has succeeded.

-----[Perform the Integrity scan-test on the JTAG DR]------------------------

This test will use blocks of 64 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.

The JTAG DR Integrity scan-test has succeeded.

[End: Spectrum Digital XDS560V2 STM TRAVELER Emulator_0]

This is the TMS320F28075.ccxml generated with the creation of a CCS SYSBIOS prorject:

<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
    <configuration XML_version="1.2" id="configuration_0">
        <instance XML_version="1.2" desc="Texas Instruments XDS100v2 USB Debug Probe" href="connections/TIXDS100v2_Connection.xml" id="Texas Instruments XDS100v2 USB Debug Probe" xml="TIXDS100v2_Connection.xml" xmlpath="connections"/>
        <connection XML_version="1.2" id="Texas Instruments XDS100v2 USB Debug Probe">
            <instance XML_version="1.2" href="drivers/tixds100v2icepick_c.xml" id="drivers" xml="tixds100v2icepick_c.xml" xmlpath="drivers"/>
            <instance XML_version="1.2" href="drivers/tixds100v2c28x.xml" id="drivers" xml="tixds100v2c28x.xml" xmlpath="drivers"/>
            <instance XML_version="1.2" href="drivers/tixds100v2cla1.xml" id="drivers" xml="tixds100v2cla1.xml" xmlpath="drivers"/>
            <instance XML_version="1.2" href="drivers/tixds100v2cs_child.xml" id="drivers" xml="tixds100v2cs_child.xml" xmlpath="drivers"/>
            <platform XML_version="1.2" id="platform_0">
                <instance XML_version="1.2" desc="TMS320F28075" href="devices/tms320f28075.xml" id="TMS320F28075" xml="tms320f28075.xml" xmlpath="devices"/>
            </platform>
        </connection>
    </configuration>
</configurations>