This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/EK-TM4C1294XL: GUI Composer

Part Number: EK-TM4C1294XL


Tool/software: Code Composer Studio

Hello,

I'm trying to design GUI features for the TM4C1294. I have both the Ethernet cable and USB port connected.

From CCS 6.2, I'm able to communicate with the device, it's recognized as COM6. But when I try to "connect" from the GUI Composer, I'm seeing an error.

It could be something basic, but I'm not able to figure it out. Also, I'm trying to find tutorials for the GUI Composer, there seems to be very limited resources available at this time. 

Any help would be greatly appreciated.

Thank you,