This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Disable specific compiler warnings

Tool/software: Code Composer Studio

I want the compiler with option -Wall to compile warning free, but have a few errors that need to be ignored.

I think there should be a pragma that does this but find no documentation/ reference.

First specific example:

1) Code that will cause an alignment error.  I want to cause the alignment error so this codes purpose is to test the error handling of misalignment  during execution...

uint64_t *llp;

uint64_t addr;

addr = (uint64_t) &addr;     -- warning: cast from pointer to integer of different size [-Wpointer-to-int-cast]
addr++;
llp = (uint64_t *)addr;          -- warning: cast to pointer from integer of different size [-Wint-to-pointer-cast]


2)  This code does not generate compiler warning but CCS shows the warning that case 1 does not have a break...

    I dont want the break..   its okay to fall through case 1 to do code in case 2.

switch (option) {

case 1 :  

doSomethingForCase1Only();

case 2 :

doSomethingForEitherCase1OrCase2()

break;

case 3:

doSomethingForCase3Only();

break;

}

}