This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/MSP430FR5994: GCC running a function from RAM

Part Number: MSP430FR5994


Tool/software: TI C/C++ Compiler

Hi all,

I am using MSP430FR59xx and I have a function that I need to run from RAM. I have been able to very easily enable this in CCS using the TI compiler by using __attribute__((ramfunc)) and in IAR by using __ramfunc. This uses a specified linker file section that is already set up to handle copying the code from FRAM to RAM at start-up, so as a user it is very simple and already done for me.

However, I need to also provide an example for GCC in CCS, and I'm having trouble finding if a similar feature exists for MSP430 GCC. Are you aware of a similar feature for the GCC compiler in CCS, and how to enable it? If not, do you have any advice on how to best implement this when using GCC?  

Regards,

Katie