Part Number: TMS320F28335
Tool/software: Code Composer Studio
Hi
This is gaurav sharma. I am working on TMS320C2000 experimental kit with F28335 Delfino family microcontroller card. I have executed a Flash LED code on the card with the help of code composer studio 6. According to the code , the third LED on the card started blinking. Even after closing the CCS6, the third LED was still blinking. It lost the control from CCS6. When i run the same code again with same target configuration then it is showing an error which is mentioned below.
Error : The program generated is not compatible with any of the CPUs in your target configuration .
Could you please me tell me ,how can i restart my controller card and how can i erase the previous build project(LED blinking).