Part Number: MSP430F5259
Other Parts Discussed in Thread: MSP430WARE
Tool/software: Code Composer Studio
Hi,
I have a working MSP430F5259 CCS project running on my desktop.
I just purchased new laptop and wanted to duplicate my working environment.
I've installed the latest versions of CCS, TI RTOS and MSP430Ware
I've built the drivers for MSP430F5259 as described here (had to tweak the *.mak file)
On my desktop I've git pushed the project and git pulled it on the laptop.
When trying to build it on the laptop I get a ton of 'catastrophic error' messages, see below an example of such error:
>> Compilation failure
Application/subdir_rules.mk:9: recipe for target 'Application/ChannelManager.obj' failed
"C:/ti/xdctools_3_32_00_06_core/packages/xdc/cfg/global.h", line 39: fatal error #1965: cannot open source file "D:/<Path-to-project>/<ProjName>-Debug/configPkg/package/cfg/<ProjName>_pe430X.h"
1 catastrophic error detected in the compilation of "../Application/ChannelManager.c".
Compilation terminated.
gmake: *** [Application/ChannelManager.obj] Error 1
'Building file: ../Application/EDFFileManager.c'
'Invoking: MSP430 Compiler'
"C:/ti/ccsv7/tools/compiler/ti-cgt-msp430_16.9.1.LTS/bin/cl430" -vmspx --data_model=restricted -Ooff --opt_for_speed=5 --use_hw_mpy=F5 --include_path="C:/ti/ccsv7/ccs_base/msp430/include" --include_path="D:/<Path-to-project>" --include_path="C:/ti/tirtos_msp43x_2_20_00_06/products/msp430_driverlib_2_70_01_01a/driverlib/MSP430F5xx_6xx" --include_path="C:/ti/ccsv7/tools/compiler/ti-cgt-msp430_16.9.1.LTS/include" --include_path="C:/ti/MSP430Ware_3_50_00_04/iqmathlib/include" --include_path="D:/<Path-to-project>/Application" --include_path="D:/<Path-to-project>/Application/NOVAlert" --include_path="D:/<Path-to-project>/Channels" --include_path="D:/<Path-to-project>/Communication" --include_path="D:/<Path-to-project>/Drivers" --include_path="D:/<Path-to-project>/Drivers/HAL" --include_path="D:/<Path-to-project>/DSP" --include_path="D:/<Path-to-shared-Project>/EDFlib" --include_path="C:/ti/msp/MSP430Ware_3_60_00_10/iqmathlib/include" --include_path="D:/<Path-to-shared-project>" --advice:power=all --advice:power_severity=suppress --define=ccs --define=MSP430WARE --define=__MSP430F5259__ --define=ADS131_16BIT_MODE --define=<ProjName> --define=xNOVALERT --undefine=_INLINE -g --printf_support=nofloat --diag_warning=225 --diag_warning=255 --diag_warning=20 --diag_warning=195 --diag_warning=827 --diag_wrap=off --display_error_number --abi=eabi --silicon_errata=CPU21 --silicon_errata=CPU22 --silicon_errata=CPU40 --preproc_with_compile --preproc_dependency="Application/EDFFileManager.d" --obj_directory="Application" --cmd_file="configPkg/compiler.opt" "../Application/EDFFileManager.c"
One thing that I noticed is that on the desktop a past MSP430Ware installation (3.50.00.04) is located directly under c:\TI, while the latest MSP430Ware installation is under C:\TI\MSP ,
I see both paths (sepcifcally iqmathlib path, see highlights above) in the error message, however I can't figure out where it comes from as the include option define it only once
Any advise as how to deal with this annoying issue is appreciated.
Thanks in advance.