Other Parts Discussed in Thread: CCSTUDIO, ENERGYTRACE
Tool/software: Code Composer Studio
I've tried both the web based and the offline version of the installer on OS X 10.12.3 (latest) and both simply launch and die.
I've installed both the latest JRE and JDK 8.121 thinking that was the issue (and rebooted even).
Then went to /var/log/system.log and found this when I launch....
Feb 1 06:57:34 jmbp17 com.apple.xpc.launchd[1] (com.apple.xpc.launchd.domain.pid.IDECacheDeleteAppExtension.98205): Path not allowed in target domain: type = pid, path = /Applications/Xcode.app/Contents/SharedFrameworks/LLDB.framework/Versions/A/XPCServices/RootDebuggingXPCService.xpc error = 147: The specified service did not ship in the requestor's bundle, origin = /Applications/Xcode.app/Contents/PlugIns/IDECacheDeleteAppExtension.appex
Feb 1 06:57:34 jmbp17 com.apple.xpc.launchd[1] (com.apple.xpc.launchd.domain.pid.IDECacheDeleteAppExtension.98205): Path not allowed in target domain: type = pid, path = /Applications/Xcode.app/Contents/Frameworks/DFRSupportKit.framework/Versions/A/XPCServices/IDETouchBarSimulatorService.xpc error = 147: The specified service did not ship in the requestor's bundle, origin = /Applications/Xcode.app/Contents/PlugIns/IDECacheDeleteAppExtension.appex
It appears as though the .zip (extracted to a folder) is incomplete. Wish this were a .dmg instead anyway.
This product is so new it doesn't have any CCS v7 FAQs, forums entries, etc (at least not that I could find), no migration pages whatever. So maybe I'm the first or I'm blind :)
Looks like CCS v7 is using Eclips 4.6 which is supposed to have CDT unit test included (which is what I'm hoping since I can't find CDT unittest for download anymore).
Please direct me to anything I'm going wrong. Thx.