This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: ICDI Debugger problems with Tiva Launchpads in CCS 6.2.0 and CCS 7.0.0/openSUSE Linux 13.2 and later

Other Parts Discussed in Thread: EK-TM4C1294XL, EK-TM4C129EXL, CC2650

Tool/software: Code Composer Studio

Hello,


I own two EK-TM4C1294XL and one EK-TM4C129EXL launchpads. When I try to debug a project to one of them, using CCS 7.0.0.00043 running in openSUSE 13.2 (tried also in Leap 42.1 and Leap 42.2, all 64 bits flavored :)), I always get the error:

CORTEX_M4_0: File Loader: Verification Failed: Values at address 0x00007FF0 do not match. Please verify target memory and memory map.

The project I used are all from TivaWare 2.1.2.111 and TivaWare 2.1.3.156. All of them get built smoothly without problems.

I also tried CCS 6.2.0.00050 but there, whenever I try to debug a project on one of these launchpads, CCS freezes. Only a hard kill closes it.

I finally tried CCS 6.1.3.00034 where all of these launchpads work fine. Every project is downloaded into the microcontroller and I am able to debug the project.

The next step I took is to connect another debugger to one of these launchpads. I used an XDS110 from a CC2650 launchpad and configured the project to use it. Everything was fine in all versions of CCS I previously mentioned.

Does anybody know some way to make CCS 7 work with the ICDI debugger?

Thank you in advance for your time,

Ilias