Other Parts Discussed in Thread: ENERGIA
Tool/software: Code Composer Studio
Hello!
I am using CCSv7 and a MSP432 launchpad (black) for C++ development. I am using gcc/g++ (4.9.3), which comes along with CCS (and I checked that it is the latest version available from the CCS App Center).
I also tried out newer compilers (g++ 6.2.4) with no success.
I have stripped down my problem to the following simple file:
#include "msp.h"
class A {
public:
A() {}
virtual ~A() {}
};
A mya;
int main(void)
{
return 0;
}
When I run this program on the MSP432 lauchpad, it immediately crashes during the start-up code. I started with a fresh CCS C Project, and renamed main.c to main.cpp. I also added the libstdc++.a library in the linker configuration. The program compiles and uploads without errors.
Some further investigations showed that the crash happens in malloc_r, when accessing an invalid address (something like 0xD000xxxx).
Can someone help me to fix this problem? I guess it has to do with the linker script (heap size?) or some other general issue concerning the gcc startup code in case of global CTORs/DTORs.
Since CCS is not providing a "New C++ Project" functionality, I am also not sure about the general C++ support in CCS.
Energia is heavily using C++, and strangely the program above works without problems in energia (which I can not use, because I don't want/need the multithreading stuff, which is mandatory there...).
Any help is highly welcome!
BR, Andreas