Part Number: TMS320C5515
Tool/software: Code Composer Studio
Hello,
My name is André and I have a problem with the Teaching ROM for C5505 eZDSP (e2e.ti.com/.../2040.c5000-teaching-rom). I'm currently using a TMS320C5515, not the C5505, but the procedures are the same for both. I'm actually trying to run some of the programs included in the ROM, but none of them seems to work. I can perfectly build them on CCS v4 and successfully connect to target (run the "Hello World" program on the board and so on), but the problem appears when I have to debug. I receive the following message:
An error was encountered when attempting to load the program.
You may continue with your debug session if you wish to attempt to resolve the issue by performing such tasks as power cycling the device or editing your startup scripts.
Continue launching?
Then if I click on "Yes", nothing happens and a red message appears in the console window saying: File is not available
I've double-checked the procedures and it's all according to the ROM!
Thanks in advance!
André