This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377D: CCS7 - Expressions Window Value column has poor formatting for structs

Part Number: TMS320F28377D

Tool/software: Code Composer Studio

CCS Gurus,

Just passing along a screenshot of the formatting I'm seeing in the Value column on CCSv7.  This is a struct which exists in the C2000 header files.

Regards,

Kris

  • Kris,

    I can see this as well in 7.0 and 6.2. When I load the same program in 6.1.3 I see {...} as the value. It seems like newer versions are expanding this for some reason. If I take a program generated by CCSv6.1.3 and load it in CCSv7 I still see the odd display so it does look to be different behavior on the debugger side. I will file a defect for someone to look into this.

    Regards,
    John