Tool/software: Code Composer Studio
I bought a new CC2650 launchpad and tried running the project 0 demo example. After i download the code on to the board it works for about 5 minutes then it says
JTAG Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.407.3) .
Cortex_M3_0: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging.
And it stops working. I'm using the XDS110 debugger