This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compile single file

In the old Code Composer V3 you could compile just the single file that was up in the editor being worked on.

Is that still possible in the new CCS V4?  There was a button to click on to do that.

  • Yes, simply right-click on the source file in the 'C/C++ Projects' view and select 'Build Selected File(s)' in the context menu.

    Thanks

    ki

  • Is there a way to configure a single keystroke to build the current file? It seems to be a basic missing feature.

    I want to just hit "Alt-f,b" without leaving the keyboard or my editor window.

    I do not want to leave the keyboard, reach over to the mouse, find the mouse cursor, make sure the projects window is visible, find the current file in a potentially very long and deep tree view, right-click, navigate a popup-menu to find the build command among 20 other items, then click back to my editor.

    BTW, Eclipse has a nasty habit of stuffing way too many items in popup menus.

    This is one of those trivial oversights, a trivial bit of code that results in a productivity disaster and a irritating little itch every time I recompile a file.

     

  • Hello,
    when I launch "Build Selected File(s)" on any ccs5 source file, I obtain:


    ...
    $(shell echo --diag_warning=225 >> ccsCompiler.opt)
    $(shell echo --mem_model:data=far >> ccsCompiler.opt)
    $(shell echo --abi=eabi >> ccsCompiler.opt)
    $(shell echo ..\..\..\..\..\..\femtoPHY_azcom\Nyquist_software\Trunk\codebase\femtoPHY\ppl\ppl_ul\ppl_ulCtrl\src\ppl_uc_UserContext.cpp >> ccsCompiler.opt)
    ${C6000_CG_ROOT}/bin/cl6x -@ccsCompiler.opt
    Internal Builder: Cannot run program "$(shell": Launching failed

    Build of selected resources is complete.


    Whole project buils is ok.
    Regards,

    Adriano