Hi,
Whenever I now attempt to load a project that I had no prior problem loading I'm getting the following error:
Multiple operations have reported errors
An internal error occurred during: "Searching for local changes".
java.lang.NullPointerException
Needless to say the project does not load.
The only work-around I've found is to first load a different project on initiating Code Composer. Once Code Composer is up I can then import the desired project without difficulty. Once the project has been successfully loaded I can then compile and link without a problem.
Any ideas as to what's causing this problem? This is the first time I've seen this.
Thanks,
Len