This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/CC2640: TI Compiler Crash

Part Number: CC2640


Tool/software: TI C/C++ Compiler

Try to compile the attached assembly code and got the following message

"C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/fastmath/qfplib-m3.s"

INTERNAL ERROR: C:\ti\ccsv6\tools\compiler\ti-cgt-arm_5.2.9\bin\armasm.exe experienced a segmentation fault

                  while processing section .text file C:/ti/simplelink/ble_cc26xx_2_01_00_44423/Components/fastmath/qfplib-m3.s line 73

This is caused by a defect in the compiler itself. TI Customer

Support may be able to suggest a workaround to avoid this.

Upgrading to the newest version of the compiler may fix this problem.

Contact TI in the E2E support forums at http://e2e.ti.com under

"Development Tools", "TI C/C++ Compiler". See the link titled

"Submitting an issue". Include this ENTIRE error message and a

copy of the .pp file created when option --preproc_with_comment

(-ppc) is used.

>> Compilation failure

gmake[1]: *** [FastMath/qfplib-m3.obj] Error 1

qfplib-m3-20160408.tar.gz