Tool/software: Code Composer Studio
I am trying to use a HEX file (generated by CCSv6) to reprogram flash during runtime. My problem is that in the 28075, the flash can only be written left-justified to a 64-bit boundary; that is, the address must end in 0 or 8. The HEX files that CCS generates do not always provide the data in left justified format (see below excerpt from my HEX file). Is there any way to tell CCS to produce a HEX file that always starts at a 64-bit boundary? If not, does TI have a recommended workaround for the 28075, whose flash must be programmed left-justified?
Thanks,
Justin
:204E00008CE29A00FE860006FE021E42761F02380E0C1EAC56650042A9420642EC09064280 [Addr: 4E00] (All along here, the addresses end in '0', which is left-justified)
:204E1000EC0A0201564100420642EDFC6F0428A901F46F029A00FE82FF690006FE028F08B6 [Addr: 4E10]
:204E2000200006C41E428F08210006C41E428F08220006C41E428F08230006C41E4202017C [Addr: 4E20]
:204E300076408DC4FE820006FE041E428748290156440042FF451E44764086A00644FE8450 [Addr: 4E30]
:204E400000060000000000000000000000000000000000000000000000000000FE041E44E8 [Addr: 4E40]
:204E5000A842064207448AA9924876408CB4FE840006761F02388A04D02A4894EF039A017A [Addr: 4E50]
:124E60006F029A020006761F02388A04D02A0694000636 [Addr: 4E60]
:204E6C00B2BD59A99B019A015CA176489D14761F02B692A1743A8BBE00069A019B017648A0 [Addr: 4E6C] (Starting here, the addresses end in 'C' this means it's not left-justified to a 64-bit boundary)
:204E7C009D209A3A76484E6C9A312B3A76484E6C9A3076484E6C923F76484E6C761F02B78C [Addr: 4E7C]
:204E8C009200FFC376489C9976484E6C761F02B7CC00000F76489C9976484E6C0006761F18 [Addr: 4E8C]
:204E9C0002B6B2BDCC3A00FF59A9FFC376489C9976484E6C92A1900F76489C9976484E6C5E [Addr: 4E9C]
:204EAC009A0D76484E6C9A0A76484E6CD0228F00C24656BF01942B0656BF010356BFC8044D [Addr: 4EAC]
:204EBC008BBE0006B2BD761F02A3592E761F02B656BF5A3F761F02B556BF092B761F02B779 [Addr: 4EBC]