Other Parts Discussed in Thread: TMS320C6748
Tool/software: Code Composer Studio
We bought CCS for use with TMS320C67xx and also the USB560v2 (BH-USB-560v2) and used them a while ago with no problem. Now I get the message
"License cannot be acquired.
The Code Composer Studio license that you are using only allows the following connection types:
- XDS100 class emulators
-MSP430 connections
-simulators
-EVM/DSKs/sZdsp kits with onboard emulation
Examples of restricted connections includes:
-XDS200, XDS510 and XDS560 emulators"
I was under the impression that having bought everything we owned it, so shouldn't get this?
Also, the "Part Number" field wont accept "TMS320C6748" so I have selected I have no part number.
Thanks for any help