Tool/software: Code Composer Studio
Got the new release of CCSV7.1 going on my Mac and linux box - It's all working really well, except for one little thing. The RTSC editor for cfg files doesn't seem to come up. When I open the cfg files, they open as a plain text file and the available products view says "The view is currently empty because there is no RTSC Configuration File open."
I have xdctools installed and registered on both systems, as well as the various rtos's, etc. I can generate various projects through the wizard, which creates a new cfg file along with the project, etc.
Using any of the examples with a pre-built cfg file, the compile even goes successfully and I can load and run the project (tcpEcho for the TM4C1294XL as an example).
It just appears that the editor for the cfg files is broken on Mac and linux.
Any thoughts here?