This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28069M: MATLAB/Simulink support for Code Composer Studio

Part Number: TMS320F28069M

Tool/software: Code Composer Studio

Is there some kind of source where I could find up-to-date information about which particular versions of MATLAB/Simulink are compatible with particular versions of Code Composer Studio. Specifically, I need to know if CCSv7 is compatible with R2016a, and in case it is not anymore, it would be nice to know if any other option is available.

  • Hi Aleksander,

    CCSv7 is NOT supported in R2016a. In fact, CCSv7.0.0 was released in December 2016, which is after MathWorks R2016a released in March 2016.

    I do know the development team is actively working on adding CCSv7 support, but I do not know when that will be complete.

    I think you can use CCSv7 to import code generated by MathWorks products, but I have not tried it. The C2000 support package still only works with CCSv6 (which is required for F2837x and F2807x).

    Some info on: processors.wiki.ti.com/.../MatLab_and_CCS

    HTH,
    -Brian