Part Number: MSP430F5529
Tool/software: Code Composer Studio
I upgraded to CCS7 and I have a number of devices installed but I dont have the MSP430. I attempted to load the software related to the MSP430 using the in software tool . I went to HELP-> INSTALL NEW SOFTWARE...then selected everything that has MSP430 .
It took 20 minutes or so for everything to get installed then I restarted the software. I went to open a new project and could not find the MSP430 devices in the "target" cell. I closed the program and restarted the computer thinking maybe this would help. But still cannot add the MSP430 compiler target configuration libraries.
Do I need to uninstall Code Composer?
How do I get this to work?
Thanks,
Chris