This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM48L952: Cannot program my Hercules development kit

Part Number: RM48L952

Hello,

Previously I've used CCS 5.5 and CCS6.1 and could program my Hercules Safety MCU development kit. The thing is that now I'm on a new PC and installed CCS7, but now it won't even find the drivers for the xds100 JTAG on board.

I've tried installing CCS7 and it didn't find the drivers, I tried uninstalling it and then installing it in administrator mode but the same thing happened.

Whenever I try connect to the board with CCS it just halts, and when I try using xds100serial.exe which is located in common/uscif I get a message telling me that there are no xds100 connected to the PC. I know the problem isn't on the board because I've been able to find it on other PCs and I've even programmed a demo application.

When I went to device manager I saw this

I've tried uninstalling and reconnecting the board several times to see if it finds the drivers, but nothing happens.

I went to ccs_base/emulation/drivers/ftdi_drivers and tried installing DPInst64.exe but it tells me that there isn't anything to install. Naturally I opened the command prompt, navigated to the same place I was and I tried running install.bat (normally and as an admin) but this is the message I get.

INFO:   Option set: dumping log info to console.
INFO:   Current working directory: 'C:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_
drivers'
INFO:   Running on path 'C:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_drivers\2.0
8.30\drv'
INFO:   No valid 'dpinst.xml' file provided.
INFO:   Install option set: Running in quiet mode. Suppressing Wizard and OS pop
ups.
INFO:   Install option set: Install all driver packages or none.
INFO:   Found driver package: 'C:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_drive
rs\2.08.30\drv\ftdibus.inf'.
INFO:   Found driver package: 'C:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_drive
rs\2.08.30\drv\ftdiport.inf'.
INFO:   Preinstalling 'c:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_drivers\2.08.
30\drv\ftdibus.inf' ...
INFO:   ENTER:  DriverPackagePreinstallW
INFO:   Driver package is already preinstalled 'c:\ti\ccsv7\ccs_base\emulation\d
rivers\ftdi_drivers\2.08.30\drv\ftdibus.inf'.
SUCCESS:c:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_drivers\2.08.30\drv\ftdibus.
inf is preinstalled.
INFO:   RETURN: DriverPackagePreinstallW  (0xB7)
INFO:   ENTER:  DriverPackageGetPathW
INFO:   RETURN: DriverPackageGetPathW  (0x0)
INFO:   Preinstalling 'c:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_drivers\2.08.
30\drv\ftdiport.inf' ...
INFO:   ENTER:  DriverPackagePreinstallW
INFO:   Driver package is already preinstalled 'c:\ti\ccsv7\ccs_base\emulation\d
rivers\ftdi_drivers\2.08.30\drv\ftdiport.inf'.
SUCCESS:c:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_drivers\2.08.30\drv\ftdiport
.inf is preinstalled.
INFO:   RETURN: DriverPackagePreinstallW  (0xB7)
INFO:   ENTER:  DriverPackageGetPathW
INFO:   RETURN: DriverPackageGetPathW  (0x0)
INFO:   ENTER:  DriverPackageInstallW
INFO:   Installing INF file 'c:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_drivers
\2.08.30\drv\ftdibus.inf' (Plug and Play).
INFO:   Looking for Model Section [FtdiHw.NTamd64]...
INFO:   No matching devices found in INF "C:\Windows\System32\DriverStore\FileRe
pository\ftdibus.inf_amd64_neutral_0a3c2df775f027fe\ftdibus.inf" on the Machine.

INFO:   No drivers installed. No devices found that match driver(s) contained in
 'C:\Windows\System32\DriverStore\FileRepository\ftdibus.inf_amd64_neutral_0a3c2
df775f027fe\ftdibus.inf'.
INFO:   RETURN: DriverPackageInstallW  (0xE000020B)
INFO:   No matching device was found for 'c:\ti\ccsv7\ccs_base\emulation\drivers
\ftdi_drivers\2.08.30\drv\ftdibus.inf'. Driver will be installed when plugged in
.
INFO:   ENTER:  DriverPackageInstallW
INFO:   Installing INF file 'c:\ti\ccsv7\ccs_base\emulation\drivers\ftdi_drivers
\2.08.30\drv\ftdiport.inf' (Plug and Play).
INFO:   Looking for Model Section [FtdiHw.NTamd64]...
INFO:   No matching devices found in INF "C:\Windows\System32\DriverStore\FileRe
pository\ftdiport.inf_amd64_neutral_0174995d0b71bf25\ftdiport.inf" on the Machin
e.
INFO:   No drivers installed. No devices found that match driver(s) contained in
 'C:\Windows\System32\DriverStore\FileRepository\ftdiport.inf_amd64_neutral_0174
995d0b71bf25\ftdiport.inf'.
INFO:   RETURN: DriverPackageInstallW  (0xE000020B)
INFO:   No matching device was found for 'c:\ti\ccsv7\ccs_base\emulation\drivers
\ftdi_drivers\2.08.30\drv\ftdiport.inf'. Driver will be installed when plugged i
n.
INFO:   Returning with code 0x200

I need to be able to program my kit, but I just can't...I haven't been able to even find the right drivers.