Other Parts Discussed in Thread: CC1310, LAUNCHXL-CC1310
Tool/software: Code Composer Studio
Hi,
I'm trying to debug a mesh radio project which involves multiple launchpads all running exactly the same code with CCS, but it won't let me have more than one instance running.
If I open another instance, it complains that the workspace is in use, then simply shows an empty window with a close button that doesn't work. image
I can't get the first instance to use another workspace either, there's only one listed and when I select 'File -> Switch Workspace -> Other...' nothing happens - the menu vanishes and CCS apparently ignores that I selected that menu item.
I'm already using another editor and CCS picks up external changes to the files just fine, why does it have this restriction on workspaces?
Furthermore, I can't find a way to select a specific launchpad in CCS. SmartRF studio seems to have this ability, why not CCS?
How can I debug multiple launchpads at once, all running the same code?
ps: why is the Part Number field saying 'Part number "LAUNCHXL-CC1310" not recognized.' ? It suggests that entry when I write cc1310...