This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Hi,
I could not find anything specific here : http://processors.wiki.ti.com/index.php/PRU_Assembly_Instructions or in ccsv6\tools\compiler\ti-cgt-pru_2.1.4\README.txt
3. MVI instruction
MVI is only supported on core revisions 2 and 3. The existing PASM assembler
supports the instruction in a limited form for v1 using pseudo operations.
http://processors.wiki.ti.com/index.php/PRU_Assembly_Instructions#Move_Register_File_Indirect_.28MVIx.29 does not talk about any restriction of having the pointer register in r1.bx (x=0..3) but
MVIB [*][&][--]REG1[++], [*][&][--]REG2[++] [, bn]
With clpru assembler, I tried following (PRU core revision = 3 )
mvib r9.b0, *r1.b0 (compiles)
mvib r9.b0, *r1.b0 (does not compile - invalid instruction)
mvib r9.b0, *r0.b0 (does not compile - invalid instruction)
mvib *r1.b0, r10.b0 (compiles)
However pasm documentation states this - I recommend to clarify this in respective clpru documentation
4.2.3.2 V2 and V3 Core Support
When using the core revision option V2 or V3, most forms of this instruction are available. The following
restrictions apply:
Register pointer registers are restricted to r1.b0, r1.b1, r1.b2, and r1.b3
The optional count parameter is not available.
I filed CODEGEN-2161 in the SDOWP system to request that the details about MVIx be updated in the wiki article you mention. You are welcome to follow it with the SDOWP link below in my signature.
Thanks and regards,
-George