This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Cannot drag and open file in CCS 7.1.0



Tool/software: Code Composer Studio

Hi there

I cannot drag and open file in CCS 7.1.0. In the previous version, I can.

How can I enable this feature?

Thanks

XIning

  • Hi Xining,
    You are simply dragging and dropping the file into the editor, correct? If so, that should still work. Nothing changed in 7.1.0 which should affect that behavior. What kind of file is it? And what host OS are you using?

    Thanks
    ki
  • I am using Windows 10. I just install the CCS 7.1.0. I think in the first 2 days, the drag and open feature worked. However, starting from yesterday, it doesn't work. When I drag the file to CCS, the mouse cursor would turn into a "stop" sign with 45 degree clockwise rotation.

    Xining