This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3200: Symbols cannot be found

Part Number: CC3200

Tool/software: Code Composer Studio

I keep running into this issue. Projects compiles & links fine, then suddenly numerous 50+ errors where symbols cannot be found.

Using CCS 6.1.200015 , part CC3200

If I clean the project and rebuild, that sometimes works as well as restarting CCS.  Now it is getting worse.

example error:

symbol 'TIMERA0_BASE' could not be resolved, main.c. 

Yet if I go to the code where TIMERA0_BASE is being used and right-click - open declaration - it takes me to hw_memmap.h

AND I have it included at the top of the file: #include "hw_memmap.h"