Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: CC3200, ENERGIA
Tool/software: Code Composer Studio
Hi Folks,
I am trying to connect my TM4C123g to a database on the cloud. I have acquired a CC3200 for this purpose.
Now I know that connection to a database is straight forward using the energia libraries but my code is written in C on CCS and I would like to continue using CCS (and C) for consistency and to have a clearer explication when presenting my work.
Is it possible to write the code to access the cloud on energia, and then use the CCS import sketch functionality to combine the code written on energia with the one that I already have (i.e., 1. is it possible? 2. do I have to use an interface between the code written on CCS and the code written on energia or a simple function call will work?)
PS: I found a piece of code written with C on an Edex online course for internet connection, but it did not -or I was not able to modify it correctly to- support enterprise internet connection. Also if there is a fix to add this functionality (connect to an entreprise internet connection) this will stop me from trying to merger energia and ccs
Also is there a particular database framework that is more friendly with TM4C chips?
Thanks,
Marwan Maalouf