Tool/software: TI C/C++ Compiler
Hi,
Let say i write a linker script to define different sections (.data, .bss, .txt), and compile it into .hex file using Code Composer studio.
a) How linker actually maps these sections in output .hex file (not a.out file, as .out can't be burn to flash.), as according to https://en.wikipedia.org/wiki/Intel_HEX, there is no sections defined inside .hex file neither there is a header to describe header sections. so why even we write these sections in linker script if they are not gonna appear in output .hex file??? Am i missing something???
b) second, if this output file is burn to some flash memory and processor like tms320c6713 is boot from this flash, how the processor gonna distinguish b/w these section even .hex doesn't contains any sections or
sections description???
Kindly correct me if i am wrong, any reference to understand these concepts will be highly appreciable.
Thanks in advance.