Part Number: TMS320F28377D
Tool/software: TI C/C++ Compiler
Hello,
I experience compiler segmentation fault when compiling for CLA.
I found this thread but i'm not using --gcc option and I tried with three different compiler version 15.x.x and 16.x.x.
This is the log message I get during compiling:
INTERNAL ERROR: C:\Prg_dev\ti\C2000_compilers\16.9.2.LTS\bin\accla.exe experienced a segmentation fault
while processing function (unknown or file scope) file (unknown) line 0
This is caused by a defect in the compiler itself. TI Customer
Support may be able to suggest a workaround to avoid this.
Upgrading to the newest version of the compiler may fix this problem.
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue". Include this ENTIRE error message and a
copy of the .pp file created when option --preproc_with_comment
(-ppc) is used.
gmake: *** [Release_CPU1\CLA_Tasks.obj] Error 1
**** Build Finished ****
Thanks for support,
Angelo