This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3200-LAUNCHXL: Connect to the XDS110 failed.

Part Number: CC3200-LAUNCHXL
Other Parts Discussed in Thread: UNIFLASH, CC3200

Tool/software: Code Composer Studio

Hello!

Then i tried "blinky" example, i got this error:

"Error connecting to the target:

(Error -260 @ 0x0)

An attempt to connect to the XDS110 failed...."

uniflash returns "Error -151"

xdsdfu -e returns "Found 0 devices" 

xds100serial returns "No XDS100.."

Out-of-the-box example works fine. FDTI drivers installed, CC3200 showed in device list as "CC3200LP JTAG Port A" and "CC3200LP UART Port B"