Part Number: TMS320F28022
Tool/software: Code Composer Studio
Win7 SP1 32bit, CCSv6.1, C2000 tools.
I am developing a project that I have put some routines into FLASH, and run others from ram.
Many times I do not change the routines or data that is already in FLASH, and in that case I would like to not erase and burn the FLASH.
Currently, I have a .h file the linker looks at and a #ifdef #else in the command file that either LOADs or NOLOADs parts depending on if I have changed that code.
Sometimes I forget to change the content of that .h file, and of course my program then goes into the weeds or I burn the FLASH unnecessarily.
Can Code Composer automatically decide for me whether to burn the flash or not?
Maybe an external routine of some kind to read the FLASH and compare it to the .out file.
Ideas?
Thanks, Mark.