Other Parts Discussed in Thread: CCSTUDIO
Hello
I have a TI DSP EMULATOR ( XDS510 USB2.0 ) .
I want to test connecting the CCStudio v3.3 to EVMOMAP-L137 with your Emulator .
I installed XDS510-USB2.0 driver and run E:\XDS510 CCS Driver \ Setup.exe and E:\CCS Software\ccs3.3\CCS_v3.3_SR11_81.6.2\CCS_v3.3_SR11_81.6.2.exe from the emulators CD.
But when I chose "F2407 XDS510 Emulator" in code composer studio setup and save it , this error appears when i am going to start CCS :
"Error initializing emulator
I/O Port = 240
Board Name: F2407 XDS510 Emulator
Cpu Name: CPU_1 "
and when i chose "F28335 XDS510 Emulator" in code composer studio setup and save it , ,the CCS will start but this error appears when i am going to connect :
" Error connecting to the target:
Error 0x00001200/-1145
Error during: OCS, Target,
Unrecoverable emulation error
I/O Port = 240
Board Name: F28335 XDS510 Emulator
Cpu Name: CPU_1 "
I have a TI DSP EMULATOR ( XDS510 USB2.0 ) .
I want to test connecting the CCStudio v3.3 to EVMOMAP-L137 with your Emulator .
I installed XDS510-USB2.0 driver and run E:\XDS510 CCS Driver \ Setup.exe and E:\CCS Software\ccs3.3\CCS_v3.3_SR11_81.6.2\CCS_v3.3_SR11_81.6.2.exe from the emulators CD.
But when I chose "F2407 XDS510 Emulator" in code composer studio setup and save it , this error appears when i am going to start CCS :
"Error initializing emulator
I/O Port = 240
Board Name: F2407 XDS510 Emulator
Cpu Name: CPU_1 "
and when i chose "F28335 XDS510 Emulator" in code composer studio setup and save it , ,the CCS will start but this error appears when i am going to connect :
" Error connecting to the target:
Error 0x00001200/-1145
Error during: OCS, Target,
Unrecoverable emulation error
I/O Port = 240
Board Name: F28335 XDS510 Emulator
Cpu Name: CPU_1 "
And when I use SDConfig and I want to Verify emulator connection ( Configuration -> Verify ), this error apeares :
>> XDS510-USB Emulator not connected/enumerated
>> Could not open emulation connection
Would you please help me ? is the problems about the CCSv3.3 driver ? how can I resolve it ?
Regards,
Zahra Mazaheri .