This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6678: Include binary with CCS project

Part Number: TMS320C6678

Tool/software: Code Composer Studio

Hi,

Is there a way to include a binary file (in this case, an FPGA binary) as part of a CCS project? I don't want to add it as a .h file because the CCS compiler expects header files to be in a certain format. I want to include the FPGA binary in the exact same format as it's compiled.

Thanks,

Viney

  • Viney,

    >>Is there a way to include a binary file (in this case, an FPGA binary) as part of a CCS project?
    There is not a direct way to include this on a project. The thread below talks about an enhancement to our build tools that unfortunately was never implemented.
    e2e.ti.com/.../89649

    >>I don't want to add it as a .h file because the CCS compiler expects header files to be in a certain format.
    Unfortunately to date there are only two methods of doing this, but only one is feasible to your particular case.
    - Directly including the .obj file into the project (impractical for your particular case)
    e2e.ti.com/.../1140537

    - Converting the binary to the header file format (the most practical way for your particular scenario)
    e2e.ti.com/.../335341

    Hope this helps,
    Rafael