Other Parts Discussed in Thread: TCI6638K2K
Tool/software: Code Composer Studio
Hello,
We capture memory transaction logs via XDS560v2 Pro Trace with the settings below:
We modified the settings for capturing DSP1 LSRAM (L2_1) EDMA WR Access only.
Our application uses EDMA_CC1_TC0 for default, and we confirmed this with the logs. But when we modify the application for using EDMA_CC4_TC0instead of EDMA_CC1_TC0, even though the register¶mset movements confirm that we are using the EDMA_CC4_TC0, memory transaction logs show that we are using EDMA_CC2_TC0.
Moreover, there is no EDMA_CC4 in the transaction master list below.
So far I am sure that there is no paramset in EDMA_CC2 which addresses DSP1 L2SRAM as destination. We are using CCS Version: 6.1.1.00022. Any suggestions about that?
Thanks in advance..