Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Hi,
When building a project on CCS V7 the gmake.exe crashes and therefore it is impossible to fully build the project (please see picture below). The project builds ok on CCS V6 with the same Code Generation Tools.
If I use the gmake.exe from CSS V6 (copy the file to C:\CCStudio_V7\ccsv7\utils\bin) the project builds ok also in CCS V7.
When gmake crashes it does this while running the post_build.bat file. The strange thing is that gmake.exe is not crashing all the time.
Operating system: Windows 7, 32Bit
CCS V7.1.0.00016
CGT: V16.9.2.LTS
Best regards,
Patrick