This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: Exporting project linker settings in ccs7



Tool/software: Code Composer Studio

I am using ccs7. For each and every project there is an option for importing and exporting project settings. That option is exporting only include path and symbols settings but not linker settings. Is it possible to export linker settings like additional library including settings?

If yes please tell me how to do that. Because in my project i need to include some static libraries. so every time i create a project, settings need to be imported and manually I need to include static library. To avoid that if exporting linker settings option is available, it will be very usefull.