I doubt this is the correct place... but I cannot find any other place to ask.
Which debug probe is for the Tiva C TMC4 ARM Launch pads? ( TM4C1294XL). Before I end up buy MORE of the incorrect parts due to incomplete descriptions and vague support information.
This page:
www.ti.com/.../TMDSEMU100v2U-ARM
Simply says:
"connects to the target board via both an ARM 20-pin and 10-pin " (I have a 20 pin Blackhawk... there is no 10 pin connector) and
" the XDS100 family features models with TI 14-pin, TI 20-pin, ARM 10-pin and ARM 20-pin connectors. Some models have dual connectors for added flexibility."
Well? HOW does one figure out which of them is which. There are NO specifications. Which are the "some" of that "some models" ?
If you scroll down, it only shows a 14 pin and 20 pin under "development tools". And yet the Tiva C TM4C1294XL uses a 10 pin JTAG.
... Still achieving a 100% failure rate attempting to get started with ANY of this family (CCS, Tiva-C, AM33xx, Piccolo... )